Riffgat - windfarm

Trenching in the winter season in a challenging environment.

Banner Riffgat w510

Riffgat HV-cable w120Project description:

  • Installation and trenching of 33 array cables.


Project challenges:

  • The work had to be performed in the winter season.
  • Requirement of minimum 1 meter burial depth.
     
Riffgat w120 Nexans' solution:
  • Capjet ® performed all infield trenching on the Riffgat project in Germany during the winter season 2012-2013.
  • All 33 cables were buried down to 1.5 meters depth and an as-trenched survey was performed by the Capjet ®.
  • The full length from windmill to windmill was protected with the Capjet, eliminating the requirement for additional protection by mattress or rockdumping.  
  • The entire project (installation and trenching) was performed with a single vessel.