Video gallery

Dubai 400 kV circuit

First 400 kV underground links in Dubai, installed by Nexans

More...

High Voltage in Qatar

Nexans is participating in the expansion of Qatar transmission Network

More...

Delma Island 132 kV

Nexans installed a submarine cable linking Delma Island to Abu Dhabi continent.

More...

DK6-First french combined cycle power station natural gas and steel gas

3 kms double circuit underground linking the station output

More...

Abu Dhabi 400 kV Link

State-of-the-art installation for the Abu Dhabi Electrical Authority

More...

Shibo 500 kV

Longest 500 kV underground link between two Shanghai substations

More...