français Login Contact Us
Global expert in cables and cabling system

About Nexans

Products and Solutions

Customer Service

Finance

Work at Nexans

News and Press

Go

Submarine Fiber Solutions

Send link to this page Your Nexans contact on this page

Submarine Fiber Solutions

 

Nexans Norway’s optical-fiber submarine cables are designed for both unrepeatered and repeatered systems and have almost unlimited capacity over long distances. Nexans Norway has a solid technology base, gained from completing more than two hundred projects worldwide and has provided more than 25.000 km cable in total. Nexans Norway cables are used for several applications: linking islands, countries, continents, between platforms, FPSOs and across and along fjords and rivers.

 

ROC-2 the world

ROC-2 the worldNexans Norway has with its newest invention, Repeatered Optical Cable, ROC-2, positioned the company as a premium partner within the submarine telecommunication industry. 

The new ROC-2 cable can connect continents with up to 12 fibers at water depths down to 8.000 meters. One fibre can transmit several terabits per second. This means that with ROC-2 more than 2 billion people can communicate simultaneously.

With its unique vault design, ROC-2 meets industry standards and is designed to withstand the requirements for transoceanic FO cables. The ROC-2 armouring range is designed to fit any sea bed conditions. To feed the repeater system, up to 10 kV can be applied to the cable with a resistance of 1 Ohm/km.

ROC-2 is built on experience gained from ROC-1, which is successfully installed and in operation between Trinidad & Tobago and Suriname and Guyana, see film to the right.

The cable has undergone extensive testing, and the complete range of ROC-2 cables are Universal Joint Consortium qualified.

The ROC-2 cable can also be used for  feeding power and telecom control signals for Oil & Gas installations.

 

URC-1

URC-1The URC-1 family of optical-fiber submarine cables have been in production since 1995 and has a history of no failures in design, materials and workmanship. It is
designed specifically for communication distances up to 500 km.

The URC-1 range is specifically designed for unrepeatered systems offering highways for services like telephony, data, video and broadcasting.

The URC-1 cable design is based on a laser welded steel tube containing the optical fibers which are embedded in jelly in a way that makes all fibers stress free, ensuring a long life time. For mechanical protection the cables may be equipped with a large variety of outer steel armour protections.

Request for quotation





Related Document
  Submarine Fiber Solutions  (4145.0kb)




 TOP
Nexans © copyright 2001 - 2012   Legal Notice | Contact Us | Site Map