Innovative Cables for Transportation and Industry

A metro line operator foils cable theft thanks to RHEYRAIL®

12/1/14

"Crime is common. Logic is rare. Therefore it is upon the logic rather than upon the crime that you should dwell."

Sherlock Holmes

More...

Enable™ Tether cables for ROVs with new high performance yarns

10/30/14

“Enhanced fibers make cables less vulnerable to failure, and prolong service life.”

More...

Why at Autoelectric, we think Henry Ford got it wrong!

10/7/14

“If I had asked people what they wanted, they would have said: faster horses.”

More...

Korean Ceramifiable® cables that can take the heat

4/29/14

And it burns, burns, burns, the ring of fire.

More...

MOTIONLINE® PROFINET cable opens new horizons for automation

2/14/14

Innovation often requires combining diverse strengths to achieve a common goal.

More...

Doubling voltages for aerospace cables

1/30/14

Every time I have gone up in an airplane, I have had the consciousness of a new discovery.

More...

Hybrid flat elevator cables reach new heights

10/18/13

Combining Nexans' separate competencies in a new product alows us to resolve complex problem.

More...

TITANEX®: Permanent innovation

4/11/13

Time passes, but good innovations persist.

More...

RHEYRAIL® tracks criminals

4/5/13

Even though we were late off the starting blocks, our careful research put us out in front.

More...

The "smart" cable that cries for help

1/24/13

 As with the human body, a skin wound calls for fast action.

More...

Enhanced jumpers for high-speed trains

1/23/13

Innovation often means stretching the imagination.

More...

To catch a thief

12/12/12

Like the red thread spun into Royal Navy ropes, coded copper tape proves cable ownership.

More...

Jumpers for extremely cold conditions

11/26/12

Innovations often arise from the interaction of neighboring market segments.

More...

A self-protective sensor

3/23/12

This unit is more than an automative sensor; it protects and stabilizes itself against malfunction.

More...

Duotrack® foils metal thieves

3/6/12

Sometimes, a technical innovation gives rise to unforeseen benefits.

More...

Some (cables) like it hot!

Transitional technologies, like hybrid vehicles, demand transitional thinking. Our innovation for high-temperature automotive power cables drew heavily on expertise from other market sectors.

More...

Railway clamps with a stroke of genius

With DuoTrack, Nexans offers an attractive solution for equipping non-electrified regional railway lines

More...

Fibre Optic cable QFCI-F1

This fire-resistant, armored optical fiber cable (QFCI) assures excellent data transmission and exceptional mechanical and environmental properties. It offers low smoke/low toxicity/low acid gas emissions under fire conditions, and can operate reliably in extreme temperatures (-40°C and +70°C) to maintain vital onboard communications and emergency systems.

More...

Crane cables get smart

10/11/11

This really is an intelligent cable - it tells us during operation if everything is OK.

More...

Nexans provides NG² with specially engineered cable for innovative PLUG shoreside power system

5/24/11

Nexans is supplying specially designed power cables to NG² for its innovative PLUG shoreside power system that makes medium-voltage power connections between shore and ship a pushbutton operation.

More...

Flexible power cable for hybrid electric vehicle

12/9/10

Innovation is often cooperative and synergistic, with the final result more than what each partner could have separately achieved.

More...

Korean car cable offers high performance

11/2/10

Rather than being perceived as a threat, a new competitive technology should be seen as an opportunity to do it better.

More...

Nexans launches ICEFLEX®

4/9/09

The first halogen free marine & offshore full range cable to resist ultra-cold Arctic temperatures down to – 50°

More...