Transrapid - Shanghai

Transrapid - Shanghai

Transrapid - Shanghai 1Project description:

  • Supply of the longstator motor winding for the 30 km Transrapid track, based on magnetic levitation technology.

Customer challenges:

  • The motor winding over the total length of the track is a key component.
  • First time use in a large scale project.

Transrapid - Shanghai2Nexans solutions:

  • A rubber-insulated 20 kV cable for stator winding with a total length of approx. 1.000 km was delivered.
  • Support the system installation by the Chinese customer in cooperation with ThyssenKrupp.